NOVO Go is an innovative, mobile telecare solution that encourages independent mobility outside the home, whilst maintaining a professional support and response service. This modality opens the doors to a whole new dimension of Technology Enabled Care.
NOVO Go is designed to give users confidence and independence in everyday life, both inside and outside the home, providing peace of mind every step of the way. It supports two-way audio communication and has an easy to press alarm button. Once activated, the device can immediately notify a responder and provide precise location details of the individual requesting assistance. NOVO Go has a modern and discreet design that can be worn on the wrist or around the neck.
Specifically designed for deployment as a professional telecare device, it is compliant with all relevant standards.
Fully integrated within the Legrand Care ecosystem and compatible with a full range of radio telecare devices.
Modern and discreet design with a simple user interface and ultra-comfortable to wear.
Can be used in a variety of different configurations to ensure that the user is kept safe and independent, both inside and outside the home.
A Plug & Play device that offers fully integrated audio communication.
With NOVO Go, we are expanding our proven professional Technology Enabled Care solutions spatially and technologically. At the touch of a button, NOVO Go establishes a voice connection to the dedicated responder or alarm receiving a home emergency call centre. To maximise efficiency, the location of the person can be determined at any time, even if no alarm has been triggered. NOVO Go delivers peace of mind for its user, at any time and in any location.
Even if the alarm has not been triggered, NOVO Go can be used as a passive mobile security device and alerting solution for those individuals with a reduced cognitive function.
Specifically designed for deployment as a professional telecare device and compliant with all relevant standards. NOVO Go is the latest technology allowing users to live more independently and safely. A small, modern, and comfortable device fully packed with features to supervise, manage, communicate, and help users both inside and outside the home. Anytime and anywhere.
Protection and maximum freedom of movement both inside and outside the home.
NOVO Go can also be used with a full range of telecare peripheral devices.
At the push of a button, NOVO Go can immediately notify a responder and provide location details of the individual requesting assistance.
NOVO Go can be used as a stand-alone mobile device, a Home Hub (including Docking Station), or in combination with a fixed Home Hub.
Dual positioning technology (GNSS & A-GPS) is used for a fast and precise location.
Radio supervision and online monitoring through the Legrand Care Cloud Management Portal.
For mobile use, NOVO Go sets standards, and in the home environment, it becomes a fully-fledged home hub by communicating with a comprehensive range of Legrand Care telecare peripheral devices.
NOVO Go can be used in a variety of different configurations to ensure that the user is kept safe and independent, both inside and outside the home.
Whilst at home, the mobile device can be placed into its docking station, creating a traditional home hub infrastructure where the user can also connect additional wellbeing devices to it. Should they wish to leave the home, they simply take the mobile device from the docking station and return it once they have safely arrived back home.
Integrated loudspeaker and extremely easy charging function.
Additional emergency call and function button.
Search function: Find my NOVO Go with DOCK.
Backup battery to always ensure NOVO Go is fully charged.
Remote configuration and firmware updates from NOVO Go.
Automatic Home / Away location function via NOVO Go DOCK or the fixed Home Hub.
Automatic activation of power saving mode functions.
Programmable GPS position update interval according to the needs of the user at all times.
Status update and event analysis on Legrand Care Cloud Management Portal.
Where a fixed home hub is permanently required in the home, NOVO Go can be used as a traditional pendant device that can activate the fixed hub. When indoors, NOVO Go knows it’s at home and preserves its battery life by only sending radio communication to the hub. If the user ventures outside, the device knows it’s away from home and turns on its mobile connectivity to function as a stand-alone unit.
Extends battery lifetime up to several months.
Fixed home hub extends home security.
Search function: Find my NOVO Go.
NOVO Go and the Fix Home Hub can always work independently too.
From day one, our NOVO Go clients benefit from all of the present and future device management functionalities of our Cloud Management Portal. In this way, they can monitor, program, and manage all NOVO Go devices remotely and in real time.
All devices and solutions are managed on one unified platform.
Numerous possibilities and enhanced functionalities.
Less training effort, more system familiarity and less driving.
Already prepared today for future technologies and requirements.
Operable from anywhere, thanks to intuitive cloud technology.
Stronger focus on core care tasks and advisory services.
Legrand Care Cloud Management Portal (CMP) combines the fixed Home Hub and mobile telecare devices under one roof with common administration and configuration of all Legrand Care devices. Due to the continued development and the creation of new interfaces, the integration of exciting new products is always possible.
Real time monitoring and status display.
NOVO Go remote programming.
Request a new position via CMP.
Detailed history of alarm and events.
Remote function updates for both NOVO Go and DOCK.
Mapping and geo-fencing capabilities.
Telephone and online support.
Our team is always looking for better ways to make an easier and better life for both clients and final users. Our technology is the most flexible, scalable and innovative because is developed based in our clients opinions and needs.
Robert-Bürkle-Straße 3
85737 Ismaning
Innovation House
Silverton Court, Cramlington,
Northumberland Business Park,
NE23 7RY
Cl. Norias, 92 - Planta 1ª.
Módulos B y C,
28221 Majadahonda (Madrid)
59 Avenue de la République
93170 Bagnolet, France
Varuvägen 2
246 42 Löddeköpinge