Direct Expansion Coolers
The DX cooling solution is available as a turn-key system meaning both the indoor unit (placed adjacent to the IT cabinets) and outdoor unit are part of the delivery. The indoor unit contains the compressor, and the outdoor unit is a remote condenser. This results in more flexibility in placement of the outdoor unit and less noise emissions compared to an outdoor unit including the compressor.

Nexpand DX10 & DX20
- Easy installation: DX cooling units are relatively easy to install and require less complex infrastructure modifications compared to other cooling technologies, such as chilled water systems.
- Suitable for various climates: DX cooling units can efficiently operate in a wide range of climates, including hot and humid environments, where other cooling technologies may face challenges.
- Low maintenance: DX cooling systems typically have fewer moving parts, resulting in lower maintenance requirements and reduced downtime for servicing.
- Perfect solution for small datacenter applications. Nexpand row-based DX units in a closed loop configuration can perfectly fit in a Micro Datacenter solution as well.
Top and Bottom Piping Connections
Connections for piping may enter the cooler from either the top or bottom of the unit. To facilitate this, all versions of the DX10 and DX20 accommodate top and bottom piping entry into the cooler. Also included on top and bottom are cable throughputs for connectivity, power and condensate discharge.
Display
The display is placed at eyesight and is seamlessly integrated in the perforated or blind doors. The latter depends on the chosen cooling configuration. It enables reading the most important values for the cooling performance, such as cold and hot aisle temperatures as well as fan speed and the degree of opening of the water valve. The standard display comes with buttons to navigate through the controller software. The display can be upgraded with a touch screen display for a more premium look and feel of the cooling solution.
Advanced Control and Carel Monitoring
To make sure you always know how the cooler is performing these are equipped with remote monitoring possibilities. Modbus RTU is standardly available as well as digital inand outputs. This will allow you to monitor and control a vast number of businesscritical parameters. Please review the list of options for more possibilities regarding remote monitoring & control.
Up to 16 DX units can be connected in a LAN Network with a maximum of 8 subgroups to work together in a functional manner (e.g. cooler rotation).
Hot Swappable Fans
The coolers are equipped with hot-swappable fans. To minimize possible downtime due to fan failure, this feature enables swift and safe replacement of the fans. The unit does not need to be turned off to replace the fan(s), so the issue of a faulty fan can be resolved in a matter of minutes
EC Fan Technology
The fans are all equipped with EC fan technology. The benefits are an extended lifetime and a significant increase in the energy efficiency of the unit. Also, the fans are equipped with emergency speed functions. This means that even with controller downtime the fans are still running
Nexpand Frame
The cooling technology is fully integrated in a Nexpand frame. In this way you benefit from the same look & feel throughout your white space solution. Baying to adjacent cabinets is done in the exact same way as baying IT cabinets.
Security
As the Coolers are based on the Nexpand platform the front and rear closure is the same as with the standard IT cabinets. Apart from keeping the same look & feel it also enables the use of the same mechanical locking possibilities as with our range of IT cabinets. With this we ensure the highest level of security possible.
Hydrophilic Coils and Integrated Float Switch
As a standard all our models feature evaporators with Hydrophilic treatment. This special coating facilitates the condensate discharge towards the drip tray which is placed below the evaporator. As an extra security feature each cooler is standardly equipped with a float switch installed in the drip tray. The purpose of the float switch is to sense when a maximum level of condensate is reached.
Slide-out Electrical Box
The electrical box is designed to take up as little space as possible without interfering with air distribution over the whole working height of the unit. To achieve this, without affecting accessibility during the initial start-up and unscheduled maintenance operations, a sliding drawer version has been created. This design also prevents tangling of the wiring whilst sliding.
Condensate Pump
When condensate discharge via gravity is not possible because of a concrete floor or other limitations, a condensate pump can be chosen. This will get rid of any condensate that may occur from the drip tray where it is collected from the heat exchanger.
Touch screen
To upgrade your cooler for a more user friendly and high-tech feeling a touch screen display can be chosen. It utilizes the same cut-out in the door as the standard display so even retrofit upgrades are an easy job..
Advanced Monitoring
When monitoring through other communications protocols is a need, we can support this by upgrading with the pCOWeb card. It features communication with SNMPv2c, BACNET, Modbus over TCP/IP and it is equipped with an integrated webserver.
Base set 100mm
When there are requirements when it comes to piping work and/or cabling underneath the cooler, a base-set which extends the height with 100mm can be deployed. The base-set is also available for our standard range of IT cabinets so the entire set-up including cooling can be perfectly aligned and have the same look & feel.
Transport Tool
Safety and ease of transportation are important factors especially in the initial stages of the cooler deployment. To ensure a safe placement of the coolers which, due to their weight and form factor, have a risk of tipping over, we have developed a dedicated transport tool. The tool is easy to mount and remove and it also improves the maneuverability of the cooler in the white space area.
Filterset G4 + Differential Pressure Sensor
To collect potential dust and particles we can offer a filter set class G4. A differential pressure sensor will detect at a pre-defined threshold when it reaches the maximum pressure. This will indicate a clogged filter so it can be replaced at the next service interval or prior to that.