Understanding UPS Efficiency for Data Centers: Part 2
In our technology-driven world, data centers are the backbone of industries like e-commerce, finance, healthcare, and communications, relying on uninterrupted power to safeguard operations and data. A critical component in maintaining this reliability is the Uninterruptible Power Supply (UPS) system. Despite its essential role, UPS efficiency often goes overlooked, even though it significantly affects operational costs and sustainability. This blog delves into the importance of UPS efficiency, how it is calculated, and the key factors influencing it in data centers.

In the first part of this series, we discussed the fundamentals of UPS efficiency—what it is, how it's calculated, and the factors that influence it. In this follow-up, we will explore the technological advancements driving UPS efficiency to new heights, and how these systems can contribute to both cost savings and sustainability in data centers.
Technological Advances Driving UPS Efficiency
One of the key technological advancements in Legrand's latest UPS system is the introduction of Silicon Carbide (SiC) power converters, which significantly enhance efficiency and performance. These are built with high-performance busbars, connectors, and power switches. Advanced controls and monitoring also ensure optimal energy usage and enable predictive diagnostics on consumable parts, keeping the system at peak performance. Additionally, dedicated controls and functionality for smart grid integration help optimize energy consumption and reduce overall power usage within the electrical grid where the UPS is installed.
SiC is a more efficient alternative to traditional silicon-based components, offering higher breakdown fields, faster switching speeds, and improved thermal conductivity. These characteristics enable UPS systems to operate at higher power densities and with greater efficiency, particularly under heavy loads.

Table 1: Si vs GaN vs SiC Comparison
Power Factor and Harmonic Distortion Impact on UPS Efficiency
A high-power factor plays a significant role in UPS efficiency. In simple terms, it measures how effectively the system uses electrical power; it is the ratio of real power (used to perform work) to apparent power (total power in the system). A power factor close to 1 indicates that nearly all the power is being converted into useful work, which is ideal for efficiency. On the other hand, harmonic distortion refers to deviations from the ideal sinusoidal waveform of the electrical power caused by non-linear loads, like UPS systems, which can distort the power waveform.
The efficiency of a UPS system is influenced by its power factor and harmonic distortion in the following ways:
Design and Components: Modern UPS systems are designed to have high power factors and low harmonic distortion. This includes the use of power factor correction (PFC) technologies and harmonic filters, which help in improving efficiency.
Energy Consumption: Improved power factor and reduced harmonics lead to lower energy consumption for the same load, translating to higher overall efficiency of the UPS system.
Operational Costs: Efficient UPS systems with high power factors and low harmonics incur lower operational costs, both in terms of energy consumption and reduced wear and tear on equipment.
In summary, new UPS systems with high power factors and low harmonic distortion levels are more efficient as they reduce power losses, enhance power quality, and minimize stress on electrical components. This results in better performance, lower energy consumption, and reduced operational costs.
Energy Consumption and Cooling Implications
One of the key benefits of improving UPS efficiency is the reduction in energy consumption, which directly impacts operating costs. A more efficient UPS generates less heat, which means lower energy usage and reduces the load on cooling systems.
Reduced Cooling Requirements: For large data centers, cooling accounts for a significant portion of operational costs. A high-efficiency UPS reduces the heat generated, reducing the need for energy-intensive cooling solutions.
Cost Savings: Even a small improvement in UPS efficiency can lead to substantial savings. For example, a 1% to 1.5% increase in efficiency in a 1 MW data center can save thousands of dollars annually, depending on the cost of electricity.
Impact on Carbon Footprint
UPS efficiency also plays a pivotal role in reducing the carbon footprint of data centers. As data centers are among the largest consumers of energy, increasing efficiency contributes to lower greenhouse gas emissions by reducing reliance on fossil fuel-generated electricity. The ripple effect of this is enormous, as lower energy consumption translates into a reduced need for cooling, further decreasing the overall environmental impact.
Practical Implications of High Efficiency for Data Centers
For data center operators, the practical benefits of high-efficiency UPS systems are multi-faceted:
Energy Savings: Higher efficiency translates into direct reductions in electricity consumption, which is especially important for large data centers operating at megawatt-scale power levels.
Sustainability Goals: Using high-efficiency UPS systems supports corporate sustainability initiatives by reducing energy waste and carbon emissions.
Operational Reliability: Efficient UPS systems are less prone to overheating and electrical stress, resulting in lower wear and tear on internal components. This leads to fewer maintenance requirements and longer operational life.
Future Trends in UPS Technology
Looking ahead, several trends are expected to further enhance UPS efficiency:
AI and Machine Learning Integration: These technologies optimize power management and enhance predictive diagnostics, helping operators identify inefficiencies and potential issues early.
Advanced Battery Technologies: Innovations like lithium-ion and solid-state batteries are expected to significantly improve UPS efficiency through better energy storage and longer life cycles.
Smart Grid Interaction: UPS systems that integrate with smart grids will enable more dynamic energy management, including demand response programs that reduce overall power consumption during peak periods.
Conclusion
As data centers continue to expand in size and complexity, optimizing UPS efficiency is essential for reducing costs and ensuring operations’ sustainability and reliability. Leveraging advanced technologies like SiC components and AI-driven power management will enable data centers to significantly improve their UPS efficiency while minimizing their environmental impact. Investing in high-efficiency UPS systems offers long-term returns in operational cost savings and enhanced reliability, making it a smart choice for data center operators worldwide.
Legrand’s Advanced UPS Solutions: Innovation, Efficiency, and Sustainability
Legrand’s new UPS solutions are designed to meet the evolving demands of data centers with cutting-edge technology, advanced power factor correction, and harmonic filtering for high-performance computing and AI environments. These systems incorporate predictive maintenance diagnostics for optimal performance and reliability while offering scalability to accommodate growing power needs. Legrand remains at the forefront of innovation by ensuring compatibility with current and emerging battery technologies and adhering to rigorous environmental standards, such as the Product Environmental Passport (PEP). Additionally, Legrand’s UPS solutions focus on sustainability by reducing Scope 1, 2, and 3 emissions, minimizing energy consumption, and lowering the overall carbon footprint of data center operations.
Need help identifying the best UPS solution? Contact Legrand for an online demo or consultation here.