Customized Containment
When designing your data center, you must consider various factors, including lighting, power management, cabling, structural elements, fire safety, and security. If your data center facility is well-optimized, you can adequately deploy a containment solution without experiencing issues with these components. However, should you need to retrofit the containment solution or have limited space that forces you to integrate everything into a more reduced footprint, you must incorporate some of these components within the containment space.
Regardless of your situation, at Legrand, we can provide a containment solution that meets your demands. The Nexpand platform offers an ecosystem where all elements are designed to provide the most energy-efficient solution, and the modulan system will allow you to construct your containment to the millimeter while integrating all required components.

Integrated cable management
Do you need cables running above your cabinets? Do they need to be at different heights or in varying positions on top of the cabinet? Whatever your cable management needs, we have a solution.

Power management in your containment
Placing power distribution above your racks has never been easier. Just define the position you need it at, and we will make it happen without interfering with any other parts of the deployment.

Customize your containment lighting
Having an existing lighting infrastructure installed in the white space before building the containment is common. If you want to increase visibility, we offer LED lights for containment, or we can integrate your own lighting.

Custom designed layout
You may have columns or beams positioned where you want to deploy your containment. At Legrand, this is not an obstacle; we can work around these structures with millimetric precision, custom designing your rack or containment layout.

Optimize access to your containment
We offer a broad portfolio of access solutions and dimensions, including mechanical or electric doors, double or single doors, sliding or saloon-type doors, and Radio Frequency Identification (RFID) locking options.
Minkels provides best-in-class containment doors for aisle widths of 1.2 and 1.8 meters, and modulan expands the portfolio with doors for aisle widths up to 3.5 meters.

A roof that adapts to your infrastructure
Whether it is a vertical or a horizontal containment, you can select transparent or translucid panels. Our horizontal containment translucid solution features FM Approved lightweight PVC panels, ideal for integration with sprinklers outside the containment, as they will fall either by temperature increase or by water accumulated on them.

Customize all elements
We can accommodate design requests in all shapes and sizes; the sky is the limit!
For example, you can request rear door access to specific network cabinets in a containment using saloon doors integrated into the side of your containment solution.
Gain the best access to your solutions, just how you need it!